Introduction: If you need to manually configure your network settings for Vention, this guide will walk you through the necessary steps. Whether you’re troubleshooting a connection issue or setting up a device, these instructions will help you ensure your laptop is correctly configured to connect to the network.
Steps:
- Access Network Connections:
- Begin by opening the Control Panel on your laptop.
- Navigate to Network and Internet > Network Connections.
- Locate your network adapter (typically named “Ethernet” or “Wi-Fi”), then right-click and select Properties.
- Select Internet Protocol Version 4 (TCP/IPv4):
- In the Ethernet Properties window, scroll down to find Internet Protocol Version 4 (TCP/IPv4).
- Ensure the checkbox next to it is checked, then click on Properties.
- Configure IP Address:
- In the Internet Protocol Version 4 (TCP/IPv4) Properties window, select Use the following IP address.
- Enter the IP address provided by your network administrator. For example:
- IP address:
192.168.7.66 - Subnet mask:
255.255.255.0
- IP address:
- Leave the Default gateway field blank unless specified by your administrator.
- DNS Server Configuration (Optional):
- If you need to specify a DNS server, select Use the following DNS server addresses and enter the preferred and alternate DNS server addresses.
- Finalize and Test:
- Click OK to save the settings and close the windows.
- Test your connection to ensure the network is working as expected.
Conclusion: Configuring your network settings manually can resolve many connectivity issues and is an essential step when setting up Vention devices. If you encounter any problems or need further assistance, don’t hesitate to reach out to our support team by sending an email to integrationsupport@vention.cc. See the below image for reference: